BQT3582601-00

Architecture

  1. The PowerLogic PFC is connected to PAS800 using RS - 485 Modbus serial cable.
  2. The CL110 sensor inside the PowerLogic PFC smart panel are discovered in PAS800.
  3. The PAS800 is connected in the network with internet accessibility to Power Monitoring Expert (PME) with firmware version 9.0 and above as a gateway server.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?