BQT3582601-00

Data Monitoring in Webpages

  1. Go to Monitoring and CL110 tab.

  2. Select PowerLogic PFC Controller or CL110.

  3. Go to Data and Advanced Data for monitoring the data parameters.

    NOTE: Alarms can be monitored from Data tab.

Enabling Alarm

Follow the below steps to enable the alarm:

  1. Go to Settings > Data Management.

  2. Click PowerLogic PFC Controller or CL110.

  3. Go to Alarm tab.

  4. Enable required alarms, click Save.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?