BQT3582601-00

CL110 Integration with PAS800

  1. Go to Settings tab > Wireless Devices > Wireless Configuration.

  2. Enable Wireless Activation. Click Save on the right bottom corner.

  3. Go to Wireless Discovery > Start.

  4. Press the push button on the side of CL110 to start the pairing process. The green LED flashes two times to show confirmation.

  5. The green LED is visible on side of the sensor, beside the push button.

  6. CL110 sensors will get discovered.

Related Topics

  • PowerLogic™ VL series PF Correction Controller User Manual: 7EN02-0375

  • Easergy CL110 Installation and Operation Manual: QGH40088

  • EcoStruxure Panel Server User Guide: DOCA0172EN

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?