BQT3582601-00

Firmware Upgrade

  1. Note the Mac ID from PAS800.
  2. Convert the last 2 bytes of MAC address from hex to decimal = YY. ZZ.
  3. The IP address for the webpage will be https:\\169.254.YY. ZZ.
  4. Connect the EcoStruxure Panel Server (PAS800) to power supply (100...277 Vac/Vdc).
  5. Go to Maintenance tab. Check if the firmware version of PAS800 is same as the latest firmware on this link https://www.se.com/us/en/product-range/40739468-ecostruxure-panel-server/#software-and-firmware. If not, follow step 6.
  6. Download the latest firmware PAS800 advanced firmware xxx.xxx.xxx for upgrade from the following link, to your local PC.
  7. Go to Maintenance > Firmware Update > Choose file from Local PC download in above step.
  8. Click Start to upload the file.
    This will take around 40 s for uploading the data.
  9. Click Install to install the new firmware.
    Do not power off the PAS800 while firmware installation is in progress.
  10. Click Restart to apply new version of firmware.
    It will take 2 minutes for the reboot.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?