BQT3582601-00

Data Logging of PowerLogic PFC and CL110 in PAS800

  1. Navigate to the Setting tab.
  2. Navigate to Data Management.
  3. Select PowerLogic PFC Controller from the device list.
  4. Enable the Data Sampling for the data parameters to be logged. Select Period for sampling.
  5. Click Save Changes.
  6. Go to Data Sampling, then click Activate Sampling.
  7. Follow above steps for CL110 data logging.
  8. Select Date and Time for exporting the data.
Related Topics
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?