Setup
- Connect the RS - 485 Modbus serial cable from PowerLogic PFC Controller to PAS800.
- Connect the LAN cable from ETH1/ETH2 port of PAS800 to the PC which is connected to same network to access the PAS800.
- Navigate the webpage with the above IP address mentioned in Firmware Upgrade.
- Skip the Login step or Enter a new Password to set for authentication.
- Pair the temperature and humidity sensor (CL110) and PowerLogic PFC Controller with PAS800. Refer Annexure: Integration of CL110 and PowerLogic PFC with PAS800.
- Place the CL110 at the locations inside the PAS800, where these parameters are to be measured and monitored.
WARNINGUNAUTHORIZED SECURITY ACCESSProtect the password from unauthorized access:- Change default passwords, since default settings are often easy to find in user manuals.
Failure to follow these instructions can result in death, serious injury, equipment damage, or permanent loss of data.
-
EcoStruxure Panel Server User Guide: DOCA0172EN
-
Technical Specification for Assemblies - CL110 Position for Smart Varset: NNZ5243200
-
CL110 Position Instruction for PowerLogic PFC NAM: GEX1696901