BQT3582601-00

PowerLogic PFC Integration with PAS800

  1. Go to Settings tab > Modbus Device > Modbus Discovery.

  2. Identify the Modbus Server ID number from the PowerLogic PFC. (Go to Menu 703 of PowerLogic PFC, by default Server ID is 1).

  3. Enter the Modbus Server ID in Selective List and Click Start. Then the PowerLogic PFC gets discovered.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?