Configuring Management Console For PAS800, PowerLogic PFC, and CL110
-
PowerLogic PFC Driver for PME 9.0
-
PowerLogic PFC Driver for PME 2020
-
PowerLogic PFC driver for PME 2022
-
CL110 Driver for PME 9.0/PME 2020
Use Management Console to add, remove, or configure system components, such as metering devices, in your Power Monitoring Expert Power Management System.
You can setup different types of sites (communication links such as Ethernet or Serial) and setup connection schedules for these sites.
Adding PowerLogic PFC, PAS800, and CL110 to Management Console
Follow the steps to add PowerLogic PFC, PAS800, and CL110 to Management Console:
-
Open Power Monitoring Expert folder.
-
Double-click the Management Console file. The Logon - Power Monitoring Expert window opens.
-
Enter User Name and Password and then click OK.
NOTE: The default User Name is Supervisor and the default Password is 0.
WARNINGUNAUTHORIZED SECURITY ACCESSProtect the password from unauthorized access:- Change default passwords, since default settings are often easy to find in user manuals.
Failure to follow these instructions can result in death, serious injury, equipment damage, or permanent loss of data.The Management Console > supervisor > Power Monitoring Expert window opens.
-
To add PAS800 as an Ethernet gateway site, follow the steps below:
-
Assign DHCP client or Static IPv4 address to PAS800 and use this for creating the Ethernet gateway site.
-
Click Sites icon and navigate to the main tab and click Edit.
-
Select Configure Site from the list, the Ethernet Gateway Site Configuration window open.
-
Enter all the details in the Ethernet Gateway Site Configuration window and click OK.
-
-
To add PowerLogic PFC as serial device, follow the steps below:
-
Click Devices icon and navigate to the main tab and click Edit.
-
Select Configure Device from the list.
The Serial Device Configuration window opens.
-
Enter all the details in the Serial Device Configuration window and click OK.
NOTE: Enter the Server ID details assigned in PAS800 web page.
-
-
To add CL110 as serial device, follow the above steps mentioned for PowerLogic PFC.
-
EcoStruxure™ Power Monitoring Expert 2022 System Guide: 7EN02-0471