Setup
- Place the two CL110 sensors in the positions identified in the CL110 LOCATIONS
- SMART VARSET document.This document is provided with the PowerLogic Smart Panel.
- Connect an Ethernet cable from your local computer to the Ethernet port 1/2 of the PAS800.
- Power on the panel server. The PAS800 takes approximately 2 minutes for starting.
- Type the default IP [ https:\\169.254.YY.ZZ ]. (Refer
to Firmware Upgrade) in the address
field of your web browser and press skip to
view the login page.
WARNINGUNAUTHORIZED SECURITY ACCESSProtect the password from unauthorized access:- Change default passwords, since default settings are often easy to find in user manuals.
Failure to follow these instructions can result in death, serious injury, equipment damage, or permanent loss of data.
-
EcoStruxure Panel Server User Guide: DOCA0172EN
-
Technical Specification for Assemblies - CL110 Position for Smart Varset: NNZ5243200
-
CL110 Position Instruction for PowerLogic PFC NAM: GEX1696901