Viewing of PowerLogic PFC and CL110 Parameters in PME
The Network Diagram in PME dashboard allows you to view the various parameters.
-
Open the Power Monitoring Expert folder.
-
Double-click the Web Applications file.
-
Enter the User Name and Password and then click OK.
NOTE: The default User Name is Supervisor and the default Password is 0.
WARNINGUNAUTHORIZED SECURITY ACCESSProtect the password from unauthorized access:- Change default passwords, since default settings are often easy to find in user manuals.
Failure to follow these instructions can result in death, serious injury, equipment damage, or permanent loss of data.The Power Monitoring Expert dashboard opens.
-
Navigate to Diagrams tab and click the Network Diagram to select the customized icon from the Diagram Library.
-
Click the icon to open the detail measurement diagram page.
-
Click the icon Click here for more VPL measurements on the bottom left of the webpage.
You will be directed to the webpage to view PowerLogic PFC real time measurement details.
-
Click Volts/Amps tab to view the real time voltage, current, power, power factor, and ambient temperature details.
-
Click the icons of Current, Power, Power Factor, and Ambient Temperature on the bottom of the webpage to view the periodically logged data.
-
If required, click Show Graph tab to view the periodically logged data in graph format.
-
Click Device Diagram tab to go back to the previous screen.
-
Click Power Quality tab to view the voltage harmonics.
-
Click Alarms tab to view the alarms settings and their status.
-
If required, click Alarm Log icon to view the pickup and dropout time of all occurred alarms.
-
Click Device Diagram tab to go back to the previous screen.
-
Click Diagnostic tab to view the settings.
NOTE: On the same page, you can also find the Serial Number and F/W Rev of the PowerLogic PFC. -
Click the icon 1 or icon 2 Click here for more CL110 measurements on the bottom left of the webpage.
You will be directed to the Monitoring window of CL110.
On the left side of the window , you can view the Temperature, Relative Humidity and Battery Voltage.
On the right side of the window, you can view the Communication Status of the Wireless Quality Indicators.
Click Logs icon on the bottom of the window to view the Historic Data Logs of Temperature and Relative Humidity.
-
Navigate to DASHBOARDS tab to view the power factor, current and temperature variations.
-
Navigate to TRENDS tab to view the details in graph format.
-
Navigate to ALARMS tab to view the alarm status of all alarm events.
You can also view the Active Alarms, Recent Alarms, Recent Events and Unacknowledged Alarms on the same page.
-
Navigate to REPORTS tab to view the report settings.