Configuring Vista for PowerLogic PFC
Vista is the PME component that displays and controls your power monitoring system. Use Vista user diagrams to display real time and logged data, monitor events and alarms, and control a variety of system functions.
Follow the steps to create PowerLogic PFC user diagrams:
-
Open Power Monitoring Expert folder.
-
Double-click the Vista file. The Logon - Power Monitoring Expert window opens.
-
Enter User Name and Password and then click OK.
NOTE: The default User Name is Supervisor and the default Password is 0.
WARNINGUNAUTHORIZED SECURITY ACCESSProtect the password from unauthorized access:- Change default passwords, since default settings are often easy to find in user manuals.
Failure to follow these instructions can result in death, serious injury, equipment damage, or permanent loss of data.The Vista > supervisor > Power Monitoring Expert window opens.
-
Go to File tab and then click Open.
-
Choose the file Equipment_GroupPage_CapBankPg1.dgm from the list and click Open.
-
The User Diagram:Equipment_Group Page_CapBankPg1 window opens.
NOTE: You can also find Equipment_GroupPage_CapBankPg1.dgm file from C:\Program Files (x86)\Schneider Electric\Power Monitoring Expert\ Config\Digrams\ud\default location. -
Go to Options tab and enable Show Toolbox to view Diagrams Objects options tab.
-
Right click on the Device Grouping Object.
The Grouping Object Configuration window opens.
-
Go to Node and select Custom. Click Select to view the list of Nodes.
-
Select PowerLogic PFC Node from the list and click OK.
You can see the Preview of the Node selected in the Grouping Object Configuration window.
-
Click OK to close the Grouping Object Configuration window.
The PowerLogic PFC Network diagram is ready for the Node selected.
-
Double-click on the Device Grouping Object to see all available data for PowerLogic PFC.
-
Go to File tab and select Save As to save the PowerLogic PFC Network diagram in a different location.
NOTE:-
You cannot save the Network diagram in the Equipment folder (C:\Program Files (x86)\ Schneider Electric\Power Monitoring Expert\Config\Digrams\ud\default).
-
Make sure that you do not disturb the existing User Diagram:Equipment_GroupPage_CapBankPg1 file (Template).
-
Related Topics
-
EcoStruxure™ Power Monitoring Expert 2022 System Guide: 7EN02-0471