Installation of PME
-
Subscribe to EcoStruxure Power Monitoring Expert (PME) with firmware version 9.0 and above using the link https://www.se.com/ww/en/faqs/home/.
-
After subscription, you will receive a link to register into EcoStruxure Power Monitoring Expert.
-
Login to the link using the registered email address and password and download the EcoStruxure Power Monitoring Expert package on your system.
Client Types
In (PME) you use clients to access the configuration tools and the applications for viewing data.
There are two different types of clients:
-
Engineering Clients are used to configure and administer the system.
-
Web Clients are used to view Power Monitoring Information.
Engineering Client
An Engineering Client is an administrative interface in (PME) that is used to configure and administer the system. Engineering Client include tool such as the Management Console, Vista, and Designer.
One Engineering Client is installed, by default on the (PME) Server.
Web Client
A Web Client is used to view power monitoring information such as real time data, historical information, and alarms which are used in everyday power management tasks.
Web Clients access the data on the server through a web browser. No installation is required.
Web Clients can run on any computer on the network. Web Clients require a Web Client license.
Web Clients can access the Web Applications (Dashboards, Diagrams, Trends, Alarms, and Reports) in (PME).
-
EcoStruxure™ Power Monitoring Expert 2022 System Guide: 7EN02-0471