Configuring Vista for CL110
Follow the steps to create CL110 user diagrams:
-
Open Power Monitoring Expert folder.
-
Double-click the Vista file. The Logon - Power Monitoring Expert window opens.
-
Enter User Name and Password and then click OK.
NOTE: The default User Name is Supervisor and the default Password is 0.
WARNINGUNAUTHORIZED SECURITY ACCESSProtect the password from unauthorized access:- Change default passwords, since default settings are often easy to find in user manuals.
Failure to follow these instructions can result in death, serious injury, equipment damage, or permanent loss of data.The Vista > supervisor > Power Monitoring Expert window opens.
-
Go to File tab and then click Open.
-
Choose the file File Equipment_GroupPage_CapBankPg1.dgm from the list and then click Open.
-
The User Diagram:Equipment_GroupPage_CapBankPg1 window opens.
NOTE: You can also find CL110_FAC_V1.0.0 file from C:\Program Files (x86)\Schneider Electric\Power Monitoring Expert\ Config\Digrams\ud\default location. -
Go to Options tab and enable Show Toolbox to view Diagrams objects options tab.
-
Right click on the Device grouping object.
The Grouping Object Configuration window opens.
-
Go to Node and select Custom. Click Select to view the list of Nodes.
-
Select CL110 Node from the list and click OK.
You can see the Preview of the Node selected in the Grouping Object Configuration window.
-
Click OK to close the Grouping Object Configuration window.
The CL110 Network diagram is ready for the Node selected.
-
Double-click on the Device grouping object to see all available data for CL110.
-
Go to File tab and select Save As to save the CL110 Network diagram in a different location.
NOTE:-
You can not save the Network diagram in the Equipment folder (C:\Program Files (x86)\ Schneider Electric\Power Monitoring Expert\Config\Digrams\ud\default).
-
Make sure that you do not disturb the existing CL110_FAC_V1.0.0 file (Template).
-
Related Topics
-
EcoStruxure™ Power Monitoring Expert 2022 System Guide: 7EN02-0471