DUG_EVlink_WSE-02

Adding schedule to tariff rate

You should add a scheduled time period for which a tariff rate will be active.
  1. Tap Add A Schedule on electricity page.
  2. Enter a schedule Name (A).
  3. Select the number of Days (B).
  4. Tap Start Time and Finish Time to set the time period (C).
  5. Tap Rate (D) and select the type of rate (Flat or Peak rate).
  6. Tap Set to save the schedule.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?