DUG_EVlink_WSE-02

Creating a schedule

The EVlink Home Smart can be controlled and triggered by a schedule. Once the schedule is set, your system will follow the active schedule. You can create or modify the schedules at any time.
  1. On the Home page, tap All devices > EVlink Home Smart.
  2. Tap Charging Mode > Customized Schedule > Add Schedule to add a schedule.
  3. Select the schedule Days (A).
  4. Set the Time (B).
  5. Tap Add (C).
    TIP: You can edit or delete the schedule by tapping on the existing schedule from the list to access the Edit Schedule menu. You can also enable Notification and Add Note.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?