DUG_EVlink_WSE-02

Using the device

The EVlink Home Smart Control Panel allows you to start and stop charging and monitor the power consumption.

On the Home page, tap All devices > EVlink Home Smart to access the control panel.

On the EVlink Home Smart control panel page, you can see the following:

  • Total cost of charging session (A).

  • Total time of charging in the session (B).

  • Total energy consumption in the session (C).

  • Start and stop charging button (D).

  • Charging Mode (E).

  • History (F).


Similarly you can control and check the current status of EVlink Home Smart from home page.

  • Start and stop charging button (G).

  • Current state of the device (H).


NOTE: Electric vehicles cannot be charged immediately after they have stopped. Reconnect the plug to start charging. Refer Connecting/disconnecting the charger.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?