Setting contract options
- Tap My Contract Options on Electricity page.
-
In the slide-up menu, select any one of the following (A):
- Time of Use (Peak/Off-Peak Hours): rate set to a specific period of time at which consumption is at its highest. It is the amount you pay for each unit of electricity consumed for the time period set.
- Flat Rate: fixed rate for the entire time period of electricity consumption.
- Spot Price Rate: standard hourly rate of electricity consumption as per tariff zone.
- No Contract: electricity rate is not set, no information related to bill will be shown in the app.
NOTE:-
By default, No Contract option is set.
-
Before changing your tariff type from peak rate to flat rate or no contract, please change charging mode from ”Cost Effective” to “Charge Now” or “Customized Schedule”.
- After selecting an option, tap Confirm.