DUG_EVlink_WSE-02

Managing the cable

  • Ensure that the charging connector and charging cable are securely stored between charging sessions.

  • Wrap the charging cable around the charging station’s cable trough.

  • If EVlink Home Smart Charger is installed indoors, protect the connector by covering it with the dust cap.

  • If EVlink Home Smart Charger is installed outdoors, store the connector by plugging it into the socket of the charger.


QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?