DUG_EVlink_WSE-02

EVlink Home Anti-tripping System

EVA1HPC1 EVA1HPC3


Overview

Home anti-tripping is a power load management system that continuously adapts the power supplied to charge the car, taking home consumption into account.
The power availability is calculated by the anti-tripping system by comparing the utility power limit and the home consumption gathered by a current transformer positioned on the bottom of the main circuit breaker.

NOTE: Anti-tripping module is designed for use with the EVlink Home charging station. Do not use with other electrical devices.

Installing Anti-tripping system

Refer to the installation instruction supplied with this product.

Installation video:

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?