DUG_EVlink_WSE-02

Tariff information

You can view and update tariff information in the Wiser app to access your energy cost and billing data.

To access tariff information:

  1. Tap on the home page.

  2. Select Home Management and select your home where the energy device is installed, to view Home Settings.

  3. On Home Settings page, select Tariff > Electricity.

    You can view and update the following in electricity menu:

    1. Contract options

    2. Tariff Zone (Only available for spot price rate contract option)

    3. Subscription type

    4. Rates (Not available for spot price rate contract option)

    5. Schedules (Only available for time of use contract option)

    Image id for LK 0001082209

  4. Once all the settings are updated, tap Save.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?