DUG_EVlink_WSE-02

Pairing the device to Wiser app

IMPORTANT: Make sure that the EVlink Home Smart charging station has been configured by an electrician.
  1. On the Home page, tap + and tap .
  2. Read the instruction and tap Next.
  3. Tap Open Camera (A) and scan the QR code located on the EVlink Home Smart.
  4. Wait for a few minutes for the app to connect and tap Done.
On successful pairing, EVlink Home Smart will appear on the Wiser app's home screen.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?