eSetup Commissioning
|
For Android mobile phones: |
For Apple mobile phones: |
![]() |
![]() |
Once the EVlink Home Smart is installed, follow the steps to commission via eSetup app:
- Open eSetup app and select EVlink Home Smart (A).
- Power on the EVlink Home Smart charger to activate the Wi-Fi® access point. The Wi-Fi® access point will remain active for 4 minutes, after power on.
- Enable Wi-Fi® on your smartphone and connect
to the EVlink Home Smart via Wi-Fi® direct.NOTE: The default PIN code to connect to EVlink Home Smart Charger is 123456.
- In eSetup app, tap Open Settings (B).
- Select EVLINK-ACCHARGER – International
- On the screen enter the New PIN, confirm the PIN
and tap Save.NOTE: The PIN must contain 6 to 16 digits, cannot contain the same digit more than 3 times, or a suit of 6 digits or more.New PIN update is successful.
- On the next page, enter the New PIN and tap Connect.
- On the firmware page, if EVlink Home Smart firmware is up to date, tap Continue to view Network Settings.
- In Network Settings page, select
the way to connect the EVlink Home Smart to the internet and tap Save and continue.
- Wi-Fi (C):Tap on Scan Wi-Fi QR Code and scan the QR code on your router to connect to Wi-Fi® automatically. Alternatively, you can choose from the list of available networks by taping Select a network or manually enter the Wi-Fi network name and password.
- Ethernet (D): Enter the network details to connect (use RJ45 cable type).
- In Electrical settings page, select the power rating
of the EVlink to match the electric installation. You can use the sliding bar (E) or –/+ to limit
the charging current and tap Save and continue (F).
- In Device settings page, you can enable or disable
the power meter using the toggle switch and
then tap Save and continue.NOTE: If you enable this option make sure you have connected the power meter to the charger.
- Tap Continue in the Supervision page.
- Once all the device settings are configured, tap Handover to customer and share the PIN with the customer.
- After sharing the PIN, tap Restart now (G) to restart the charger.
Please wait for 5 minutes before EVlink Home Smart connects to the internet router.EVlink Home Smart shall be restarted according to the applied configuration.NOTE: In case you need to modify the commissioning parameters, you can reconnect to EVlink Home Smart to eSetup during the 4 minutes, after restart or power on. - The LED will turn to solid green 5 minutes after restart confirming that EVlink Home Smart is successfully connected for remote operation.
-
Refer Pairing the device to pair with Wiser app.
-
Refer Using the device to monitor and control using Wiser app.