DUG_EVlink_WSE-02

Tariff rate

You can add flat and peak rate value in the Wiser app.

Adding Flat Rate

When My Contract Options is set to Flat Rate:

  1. In the Rates section, tap Flat Rate.

  2. Enter the Rate and then tap Set.

Adding Time of Use (Peak /Off-Peak Hours)

When My Contract Options is set to Time of Use (Peak /Off-Peak Hours):

  1. In the Rates section, tap Peak Rate.

  2. Enter the Rate and then tap Set.

Adding Rate

  1. Tap Add Rate on electricity page.

  2. Enter name (A) and rate per kWh (B), then tap Set.

TIP: You can set the highest tariff rate as a peak rate and other tariff rates as an off-peak rate.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?