DUG_EVlink_WSE-02

Using stop button

EVlink Home Smart has a stop button to cut off electricity if the connection cannot be shut down normally.


NOTE: Stop button can also be used to reset the PIN by rotating it 90° clockwise. Refer resetting the PIN.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?