Calibration
-
Before using this device for the first time, it must be calibrated, or you can adjust its duration manually.
-
Do not use the shutter either manually or on the app during calibration to avoid interruption.
Shutter calibrating
To
calibrate the run time manually:
-
On the device control panel page, tap .
-
On the slide-up menu, you can set the run time manually using +/- button or using the sliding bar (A) and then tap Confirm.
NOTE: To determine the default run time, record the time it takes to fully open/close the shutter (edge to edge).
To calibrate the run time using app:
-
In , tap Calibration (B).
-
On the slide-up menu, select the calibration start point (C):
– Start from the top: The shutter will move from top to bottom (closing).
– Start From the bottom: The shutter will move from bottom to top (opening). -
Wait until the shutter reaches its starting point and then tap Start.
-
Tap Done (D) once the shutter reaches other end.
The app displays the progress of calibration. -
Once the process is complete, tap Tilt Calibration on the pop-up window for shutter slat calibration.
Slat tilt angle calibration
To calibrate
slat tilt angle:
-
On the Settings page, tap Slat Tilt Angle for slide-up menu.
-
Select tilt type (A) based on the motor installed and then tap Confirm:
-
90 Slat Rotation
-
180 Slat Rotation
-
Not Supported
-
Blind
IMPORTANT: If the shutter is installed with a non rotating slat or blind, the calibration process is complete, and no further steps to follow. -
-
Read the pop-up notification and tap Confirm.
-
Make sure the shutter is in fully closed state and tap Prepare.
-
Select the check box (B) and tap Start.
-
Tap Stop (C) to finish calibration.
TIP: You can retake the calibration by tapping Reset. -
Tap Done once the process is complete.
The app displays the progress of calibration.TIP: You can set the run time manually by taping
Duration Adjustment (D).