DUG_Push-button Module_WSE-02

Creating a schedule

The device can be fully controlled by schedule. Once the schedule is set, the device operate at a given time.
  1. On the Home page, Tap All devices > 1G Shutter.
  2. Tap Schedule > Add Schedule to add a schedule.
  3. In Add Schedule menu, set the time (A).
  4. Tap Repeat (B) to select the days you want to set the schedule.
  5. Tap Note (C), enter the note and tap Confirm.
  6. Tap the toggle switch (D) to turn On the Notification for the schedule. The app will send a notification that the scheduled task is executed at the time of schedule.
  7. In Percentage (E) and drag the sliding bar to adjust or Open/Close the shutter.

  8. Tap Save.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?