DUG_Push-button Module_WSE-02

Pairing Wireless Switch with Push-button Module

  1. Short press the upper push button 5 times in quick succession on the Wireless switch.
    The status LED blinks green.

  2. Short press the push-button module 5 times in quick succession.

    Upon successful pairing, the green LED on the Wireless switch and the push-button module will stop blinking. When the push-button module is connected to the relay or dimmer insert, the connected light blinks for a few times. Similarly, if the push-button module is connected to the shutter insert, the shutter moves up and down for a few times.

You can also use the following scenarios to pair a Wireless switch with a push-button module:

  • 1-gang Wireless switch (B) with 1-gang push-button module (A): Pair the Wireless switch with the push-button module.

  • 1-gang Wireless switch (B) with 2-gang push-button module (A): Pair the Wireless switch with either the left or right push-button module. You can also pair another rocker of the push-button module with another Wireless switch.

  • 2-gang Wireless switch (B) with 1-gang push-button module (A): Pair either the left or right Wireless switch with the push-button module. You can also pair another rocker of the Wireless switch with another push-button module.

  • 2-gang Wireless switch (B) with 2-gang push-button module (A): Pair the left Wireless switch with either the left or right push-button module, or the right Wireless switch with either the left or right push-button module.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?