DUG_Push-button Module_WSE-02

Backlight mode

You can select the LED indicator mode for easy identification of the device status.
  1. On the Home page, tap All devices > 1G Switch.
  2. On the device control panel page, tap Settings.
  3. Tap Backlight Mode (A) and select any one of the following:
    • Reverse with Load - The LED on the switch is turned on when the device is turned off.
    • Consistent with Load - The LED on the switch is turned on when the device is turned on.
    • Always Off - The LED on the switch is always turned off.
    • Always On - The LED on the switch is always turned on.

    For information on LED color during each modes, refer to LED Indication.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?