DUG_Push-button Module_WSE-02

Resetting the device

You can reset the Push-button module to the factory default manually at any time.

Short press the top-center push-button 3 times and hold for 10 seconds to reset the device to the factory default mode.


TIP: In case of the 2-gang Push-button module, short press the top-right push-button 3 times and hold for 10 seconds to reset the device to the factory default mode.
NOTE: All data related to configuration, users, and the network are deleted completely.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?