DUG_Push-button Module_WSE-02

Removing the device

You can remove a device from the Wiser system using app.
  1. On the Home page, select the device for which you wish to remove.
  2. At the top-right corner of the screen, tap .
  3. Tap Remove and Factory Reset Device.
    TIP: On the home page, you can tap and hold the devise button to remove from Wiser system.
    NOTE: By removing the device, you will reset the device. If you still have a problem with the reset, then refer to resetting the device.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?