DUG_Push-button Module_WSE-02

Pairing device with auto scan

Pairing the device with auto scan automatically discovers the device when the corresponding device is powered On.
  1. On the Home page, tap +.
  2. Tap Auto scan > Confirm > Start scanning.
  3. If you have one hub proceed to step 5, if you have multiple hubs then proceed to step 4.
  4. Tap Select hub and select the Wiser Hub from the slide-up menu.
  5. Short press the top right key 3 times to start the pairing process.
    Wait for a few seconds until the device search is completed.
    NOTE: If you want to pair multiple devices at once, perform step 5 on each device and wait for a few seconds.
  6. Select 1G Switch and tap Next.

  7. Tap Done once the device is added successfully.
    NOTE: Pairing the device is shown with a 1-gang device as an example. The same process is appealable for the other 1G/2G Switch, Dimmer, and Shutter.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?