DUG_Push-button Module_WSE-02

Operating the device using app

You can open\close the shutter using the Wiser app.
  1. On the Home page, Tap All devices.
  2. In 1G Shutter Tap on for slide-up menu.
  3. On the slide up menu select Open/Close to operate the shutter.
    NOTE: You can navigate to the control panel of the device to preform the operation. The control panel shows the current state of the device.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?