About the device
The Push-button module can be completed with:
-
corresponding 1-gang or 2-gang rockers
-
Frame in the corresponding design
-
corresponding inserts for switch, dimmer, and shutter or blind control
Insert Supported Gang 1 Gang 2 Gang Switch Relay switch inserts ü ü Dimmer Universal dimmer inserts ü ü 1-10 V insert ü X DALI insert ü X Shutter Blind control insert ü X
Features of a push-button module
-
The Push-button module supports functionality such as switching, dimming and shutter control.
-
With the Wiser app, you can combine the settings of one or more devices to form a Moment or an Automation.
-
You can create a schedule for the various device functions in an easy manner as per your specific requirements for comfort and convenience.
1-gang, combination of:
-
This device user guide shows pairing, configuration and other features of the 1-gang switch, dimmer, and shutter or blind control. The same can be done for the 2-gang supported device.
-
The 1 gang push-button module can only be combined with 1 gang insert, and 2-gang push-button module only with 2 gang insert. No combination of 1 gang push-button module with 2 gang insert.