DUG_Push-button Module_WSE-02

Pairing device manually

You can pair the device to Wiser system manually with or without installed code.
  1. On the Home page, tap +.
  2. Tap , select the Wiser Hub on the slide-up menu.
  3. Select an option to add the device (A):
    • Add Device with Install Code
    • Add Device without Install Code

    TIP: It is highly recommended to add the device with install code.
  4. To pair the device with install code, tap Add Device with Install Code to display the slide-up menu. Select any one of the options (B):
    • Scan Install Code - you can scan the device for the install code. Position your camera to scan the QR code or barcode available on the device.
    • Enter Install Code Manually - you can manually enter the install code on the device.
    After adding the device with Install Code, proceed to Step 6.

  5. To pair the device without install code, tap Add Device without Install Code.
  6. Short press at the right top corner 3 times.
    LED blinks orange.
  7. In the app, select Confirm that the LED is blinking (C) and tap Start configuration.

  8. After a few seconds, a solid green LED indicates that the device is successfully paired to the Gateway/Hub

  9. Once the device is added in the app, tap Done.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?