DUG_Push-button Module_WSE-02

Shutter control

NOTE: Shutter will function only with 1-gang Push-button module only.

On the Home page, tap All devices > 1G Shutter to access the control panel.

On the control panel page, you can see the following:

  • The current state of the device (A)

  • Control button (B)

  • Slat position control (C)

  • Schedule (D)

  • Settings (E)


QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?