DUG_Push-button Module_WSE-02

Switching/Dimming the device using app

You can switch on/off and increase/decrease the brightness of the device.

Switch on/off the device

To switch on/off the device:

  • On the Home page, tap the power button (A) to switch on/off the dimmer.

  • You can also navigate to the control panel of the device and tap to switch on/off the dimmer.

    NOTE: The control panel shows the current state of the dimmer.

Adjusting the brightness of the device

To increase/decrease the brightness of the device:

  • On the Home page, tap the ˅ (B) for common function and drag the slider to adjust the brightness of the dimmer.

  • You can navigate to the control panel of the device and drag the sliding bar up/down to increase/decrease the brightness.

    NOTE: The control panel shows the current brightness percentage of the dimmer.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?