DUG_Schneider Charge_WH-03

For your safety

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION OR ARC FLASH
  • The equipment must be installed, commissioned, serviced, and maintained only by qualified personnel.
  • The charger, the cable and the connector must be regularly checked by to detect any potential damage (visual inspection).
  • In case the charger is damaged, it must be immediately turned off and replaced.
  • Do not open or modify the charger.
Failure to follow these instructions will result in death or serious injury.
WARNING
RISK OF INJURY
  • Do not use any extension cable to connect the charger to the electric vehicle.
  • Do not connect any other type of loads to the charger (power tools, etc.). Only connect electric vehicles or their charging equipment.
  • Do not use brute force to unplug the charging connector from the Electric Vehicle as it is mechanically locked.
  • Prevent the connector to be in contact with heat source, dirt or water.
  • When using an integrated charger to charge your electric car, please read the vehicle's tips and instructions carefully.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
CAUTION
RISK OF DAMAGING THE CHARGING STATION
Never clean the charging point by spraying it with water (Hose for garden watering, high pressure cleaners, etc)
Failure to follow these instructions can result in injury or equipment damage.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?