UG_Wiser Building Management System_WH-00

Home Screen

You will land on the Home page once you log in to the Wiser BMS.

Here is an example of the home screen of the Wiser BMS. As a building manager, you can request a different layout for your dashboards. The following example shows the standard layout, which will be adapted to the building's picture and floor plans.

Overview of the Home Screen:

A

Home

Takes you to the Home page.

B

Number of Alarms

Displays the number of alarms created.

C

Wiser Status

Indicates whether the system is connected to Wiser.

D

Average Rooms Temperature

Shows the average temperature of all rooms.

E

Average Set Point Rooms

Displays the average set point for all rooms.

F

Weather

Provides the forecast, including day/night conditions, outside temperature, wind, and humidity.

G

Floorplan

Shows the floorplan and how devices are set up. For more details, refer to the floor plan topic.

H

Alarms

Allows you to create alarms for devices. For more details, refer to the alarms topic.

I

Trends

Displays trends based on energy consumption. For more details, refer to the trends topic.

J

Energy Dashboard

Shows the energy dashboard with flow charts. Form more details, refer to the energy dashboard topic.

K

Alarm Notifications

Displays alarm notifications.

L

Profile

Allows you to set workspaces, options, and user settings.

M

Local

Displays the date and time.

N

Building Image

Displays the building image. When you hover over it, the floorplan for that floor is highlighted.

O

Back to Overview

Allows you to return to the home screen when you are on other tabs.

P

Hamburger Menu

Displays all notifications such as alarms, schedule, etc.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.