UG_Wiser Building Management System_WH-00

Creating a Schedule

  1. Select a room in the floorplan layout.
    The selected room screen appears.
  2. Click Schedule.
    The Wiser Schedule screen appears.
  3. Select the day and click + (A) to create a schedule.
  4. Select the Temperature (B).
  5. Set When (C) the event must occur.
  6. Click Set (D) to save the event.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.