UG_Wiser Building Management System_WH-00

Changing the Regional Settings

You can change the Regional Settings in the User Settings.
  1. On the top-right pane, click Profile.
  2. Click Options.
  3. Click Regional Settings.
  4. In the Language list, select the language.
  5. In the Date, time and number format list, select the date, time and number format.
  6. In the System of measurement list, select the system of measurement.
  7. In the Decimal list, select the number of decimals.
  8. In the Relative Time list, select if you want to use relative time.
  9. Click OK.
You have successfully changed the regional settings.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.