UG_Wiser Building Management System_WH-00

Supporting Devices

Wiser BMS is compatible with both the 1st and 2nd generation Wiser Hubs. You can use all Wiser Home devices with Wiser BMS.

NOTE: It is highly recommended to use mains-powered thermostats. For example, if the Wiser system is installed in dwellings where tenants are not available to replace batteries, it is recommended to install mains-powered devices, such as the Wiser flush-mounted thermostats.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.