UG_Wiser Building Management System_WH-00

Changing the Theme Settings

You can change the Theme Settings in the User Settings.
  1. On the top-right pane, click Profile.
  2. Click Options.
  3. Click Theme Settings.
  4. In the Dark Mode field, select if you want to use dark mode.
  5. In the Size Mode field, select the size of icons and fonts.
  6. Click OK.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.