UG_Wiser Building Management System_WH-00

Alarms

The alarm allows you to notify of important events and issues with the building management system. You can set an alarm for notifying overconsumption or no consumption of the specific device.

  • You can use an alarm to alert you if the monitored variable matches the configured alarm conditions.

  • You can configure an alarm to send a notification when the alarm is triggered. You can also configure the alarm to flash and play a sound when it is triggered.

  • For example, you can create an alarm for when the set point temperature of a room exceeds 25 degrees during the summer season. Once the temperature crosses 25 degrees, the system will trigger an alarm and send a notification.

The following image is an example of a notification triggered when the conditions are met.

Navigating to the Alarms

  1. On the Home screen, click Alarms.

    You can see the Alarms screen where the notifications are displayed.

TIP: You can also find notifications by clicking the on the top-right pane.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.