UG_Wiser Building Management System_WH-00

Profile Settings

You can set workspaces, options, and user settings.
  1. On the top-right pane, click Profile.

  2. You can see the following options:

    • Workspaces (A)

    • Options (B)

Workspaces (A)

Workspaces (A)

Allows you to switch between different workspaces if you are monitoring multiple buildings.

Fullscreen (C)

To maximize the screen view.

Help (D)

To access help resources.

Log off (E)

To log off from the application.

Options (B)

Change password (F)

Allows you to change your password.

User settings (G)

Allows you to change regional and theme settings.

About (H)

Provides information about the application.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.