UG_Wiser Building Management System_WH-00

Navigating the Floorplan

The Schneider Electric team creates the floorplan based on the building manager's requirements. Once the floorplan is ready and devices are set up, you can check the floorplan to see the number assigned to each room. You can also check the temperature settings, turn devices ON or OFF remotely, and create schedules.

  1. On the Home screen, click Floorplan.

  2. On the left pane, you can see the following options:

    • Building Overview

    • Floorplan

Building Overview

The Building Overview displays a complete image of the building. When you hover over different areas of the building image, the corresponding floorplan is highlighted, indicating the specific floor.

Interactive Floorplan: Hovering over the building image highlights the floorplan, making it easy to identify different floors and their layouts.

Navigation: Clicking on the highlighted floorplan redirects you to the Floorplan tab, where you can view detailed information and manage devices for that specific floor.

System Status: Provides a quick overview of the operational status of various building systems, such as HVAC, lighting, and security.

Floorplan

You can see all rooms assigned with room numbers. When you hover over a room, it will be highlighted, indicating that the room is assigned a number and devices are set up.

Here is an example of a standard floor plan layout:

Changing the Set Point Temperatures
  1. Select the room in the floorplan layout.

    The selected room screen appears.

  2. In the Set Point section, click +/- to increase or decrease the temperature.

TIP: If a room is equipped with a relay switch, dimmer, or socket, you can see the ON/OFF button as well.
Room Screen Details

Overview of the selected room:

A

Schedule

To create a schedule for the room. For more details, refer to the schedule topic.

B

Current Temperature

Displays the current temperature of the room.

C

Set Point

Increase or decrease the temperature by clicking the +/- buttons.

D

Connection Status

Displays the connection status of the room.

E

Battery Level

Displays the battery percentage.

F

Devices

Displays the number of devices set up in the room.

NOTE: The graphical style of the Room Control widget can vary and be localized according to the country or customer preferences.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.