SUG_Wiser_Home_UK_IRL_WH-05

Appliances

Wiser Smart Plug

WB704H1A0902

Remotely control and monitor the power consumption of the plugged-in load.

Instruction Sheet (PDF)

Device User Guide

Wiser Power Micromodule

CCTFR6730

The Wiser Power Micromodule hereinafter referred as module is for switching loads (up to 3000 W resistive) such as a hot water tank or a socket outlet.

In combination with the Wiser app, the energy consumption can be measured and the module can be used for load shedding or demand response.

Instruction Sheet (PDF)

Device User Guide

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.