Google Home
Google Home is a brand of smart speakers that work similarly to Amazon Echo. Google’s intelligent PA, Google Assistant, is equivalent to Amazon’s Alexa. Google Home is also available on all Android devices and does not require the use of the ‘Smart Speakers’.
The user can speak a profusion of commands to request information, or ask the Google Assistant to perform an action such as play music, video playback, report news, access home automation. All of this can all be controlled from a Google Home device.
Configuring Wiser Home with Google Home
-
Tap view the available cloud services.
-
Tap on Google Assistant . This will open the Google Assistant app on your smartphone to link it with the Wiser system.
-
Select Wiser Heat from the list to configure your Wiser Home setup.
-
Enter the username and password you created for your Wiser system, and tap Done.
-
Grant the required permissions to allow you to discover all the Wiser devices you have setup, and to control your wiser system using google assistant app and by using voice command.
Changes made with Google Home
All changes made through a voice command related to room thermostats and radiator thermostats are valid for one hour, or until the next scheduled event. The user cannot change this action. This also applies for boosts initiated from the radiator thermostat.
The reason for not implementing permanent changes to Wiser temperature is that a voice command can easily be forgotten, resulting in the heating accidentally being left ON for long periods of time, such as when users exit their home.
Common Wiser commands for Google Home
Listed below are common Wiser commands used with Google Home:
-
Enquiry: “OK Google, is the light in bedroom ON?”
-
Room Temperature: “OK Google, how warm is (room name)?”
-
Set Temperature: “OK Google, set (room name) to XX degrees”
-
Increase Temperature: “OK Google, increase setpoint by XX degrees”
Listed below are common Wiser Smart Plug commands used with Google Home:
-
Table lamp command: “OK Google, turn ON/ OFF the Table lamp”