SUG_Wiser_Home_UK_IRL_WH-05

Hub

1st Generation Hub

Wiser HubR (Channel 1)

WT714R1S0902

Wiser HubR (Channel 2/3)

WT724R1S0902

WT734R1S0902

The Wiser HubR is used to connect the Wiser devices. This version is used where central heating (e.g. boiler or heat pump) is used.

The Wiser HubR is available in three variants, according to your heating system

  • One Channel (WT714R1S0902): 1x heating, for combination boilers.

  • Two Channels (WT724R1S0902): 1x Heating, 1x Hot water, for conventional boilers with a separate hot water cylinder

  • Three Channels (WT734R1S0902): 2x Heating, 1x Hot water, for large properties with dual heating circuits.

Instruction Sheet

Getting to know the Hub

2nd Generation Hub

Wiser Hub 2nd Generation

CCT501800

The Wiser Hub 2nd Generation monitors and controls the Devices of your Home via the Wiser Home App. It is connected to the Wiser Cloud for remote control via Wi-Fi®.

Instruction Sheet (PDF)

Getting to know the Hub

Wiser HubR 2nd Generation (Channel 1)

CCTFR6311G2D

Wiser HubR 2nd Generation (Channel 2/3)

CCTFR6312G2D

CCTFR6313G2D

The Wiser HubR 2nd Generation is the central control unit of the Wiser Home system. It monitors and controls the devices of your home via the Wiser Home app. It can directly control a heating system and turn on a boiler.

The Wiser HubR 2nd Generation is available in three variants, according to your heating system

  • One Channel (CCTFR6311G2D): 1x heating, for combination boilers.

  • Two Channels (CCTFR6312G2D): 1x Heating, 1x Hot water, for conventional boilers with a separate hot water cylinder

  • Three Channels (CCTFR6313G2D): 2x Heating, 1x Hot water, for large properties with dual heating circuits.

Instruction Sheet (PDF)

Getting to know the Hub

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.