SUG_Wiser_Home_UK_IRL_WH-04

Kits

Wiser HubR (1st Generation)

Wiser Thermostat Kit 1

WT714R9K0902

1 x Wiser HubR (1st Generation) Channel 1

1 x Wiser Room Thermostat

One channel thermostat pack ideal for combi-boilers. Enables you to control heating via the Wiser Home app.

Instruction Sheet

Device User Guide (Wiser Room Thermostat)

Wiser Thermostat Kit 2

WT724R9K0902

1 x Wiser HubR (1st Generation) Channel 2

1 x Wiser Room Thermostat

Two channel thermostat pack ideal for conventional systems. Enables you to control heating and hot water via the Wiser Home app. Wire in existing cylinder thermostat for hot water control.

Instruction Sheet

Device User Guide (Wiser Room Thermostat)

Wiser Thermostat Kit 3

WT734R9K0902

1 x Wiser HubR (1st Generation) Channel 3

2 x Wiser Room Thermostat

Three channel thermostat pack ideal for properties with two heating zones. Enables you to control heating and hot water via the Wiser Home app. Wire in existing cylinder thermostat for hot water control.

Instruction Sheet

Device User Guide (Wiser Room Thermostat)

Wiser Multi-zone Kit 1

WV714R9K0902

1 x Wiser HubR (1st Generation) Channel 1

2 x Wiser Radiator Thermostat

1 x Wiser Room Thermostat

One channel thermostat system with two radiator thermostats to start zoning your system. Suitable for combination boilers. Control the room thermostat and radiator thermostats via the Wiser Home app. Add more radiator thermostats to create more independent zones.

Instruction Sheet

Device User Guide (Wiser Radiator Thermostat)

Device User Guide (Wiser Room Thermostat)

Wiser Multi-zone Kit 2

WV724R9K0902

1 x Wiser HubR (1st Generation) Channel 2

2 x Wiser Radiator Thermostat

1 x Wiser Room Thermostat

Two channel thermostat system with two radiator thermostats to start zoning your system. Suitable for conventional boilers. Set schedules for the room thermostat, radiator thermostats and hot water via the Wiser Home app. Add more radiator thermostats to create more independent zones.

Instruction Sheet

Device User Guide (Wiser Radiator Thermostat)

Device User Guide (Wiser Room Thermostat)

Wiser Hub 2nd Generation

Wiser ASHP Kit

Wiser ASHP Kit – Daikin Altherma

CCTFR6900DND

Wiser ASHP Kit – Panasonic Aquarea

CCTFR6900PCD

1 x Wiser Hub 2nd Generation

1 x Aidoo Pro Heat Pump (Wiser ASHP Interface)

1 x Wiser ASHP Interface – Ext Cable

This kit is purely for air to water heat pumps. It is a solution that lets you control the heat pump through the Wiser Home app. An Wiser ASHP interface is wired to the heat pump and connects to the Wiser Home app via Wi-Fi®.

Instruction Sheet (PDF)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.