SUG_Wiser_Home_UK_IRL_WH-04

Eco Mode

Eco Mode is a smart feature designed to maximise the efficiency of your heating system. It automatically optimises the stop time of the heating phase, each time the set temperature changes from a higher to lower value.
NOTE: Eco Mode is a system feature that is either activated or deactivated for all rooms.
NOTE: Eco Mode feature will not activate when cooling Mode.

Eco Mode deactivated

Wiser switches the set-point temperature at 10 pm according to the schedule. Depending on the weather and how well-insulated the home is, the room temperature drops proportionally starting at 10 pm.

The boiler keeps cycling until 10 pm.

Eco Mode activated

When Eco Mode is activated, Wiser establishes how well your home retains heat in relation to the current and predicted outdoor temperatures. Based on this, the system switches to the next scheduled set-point temperature before 10 pm without any noticeable loss of comfort.

The period between the time that Eco Mode switches the set-point and 10 pm represents the eco period, and savings occur as a result of the boiler not being switched ON.

The boiler stops firing before 10 pm.

When a room is in an Eco period, an ECO icon will appear in the room on the home screen.

The ECO icon will also be visible on the temperature adjustment screen and the room thermostat.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?